Registered Users Member

Lampe Philips HUE

Bonjour,

Je voulais savoir si dans les prochaines mises a jour il y aura une compatibilités avec les lampes Philips HUE?

  • In reply to renogen2.0@outlook.fr:

    Bonjour,

    Actuellement, les télécommandes et les détecteurs ne sont pas compatibles avec Energeasy Connect.

    Bonne journée
  • In reply to Nico85:

    At the present time, drugs generated by compounding pharmacies are not regulated by the FDA, which has various public health organizations and opponents of the death penalty concerned about the safety of its usage. Furthermore, once the names of compounding pharmacies are revealed, they risk facing public outrage, such as one pharmacy did when it received hate mail and negative publicity from local media outlets.
    Maya Foa, director of Reprieve's death penalty team, said compounding nembutal pills for sale online nembutal pills for sale online pharmacies are in the industry of improving the health and lives of patients rather than becoming the "henchman" for state governments.https://hospitableending.com/
    "Why should compounders be forced to now play henchman to the ever-hungry executioner," said Foa. "Good compounders want to improve the lives and health of patients; they don't wish to be mired in execution drug controversies, forced to mix drugs to kill prisoners in dangerous and experimental executions."
  • In reply to renogen2.0@outlook.fr:

    Bonjour,

    Les télécommandes et détecteurs ne remontent pas sur notre système.
    Ils sont utilisable en local via l'application Hue directement.

    Ronan
Recommended