Registered Users Member

PROBLÈME COMMANDE

Bonjour.

Je ne peux plus piloter mon installation depuis mon Iphone.

Quelle solution !!!!

Fred.S

  • At the present time, drugs generated by compounding pharmacies are not regulated by the FDA, which has various public health organizations and opponents of the death penalty concerned about the safety of its usage. Furthermore, once the names of compounding pharmacies are revealed, they risk facing public outrage, such as one pharmacy did when it received hate mail and negative publicity from local media outlets.
    Maya Foa, director of Reprieve's death penalty team, said compounding nembutal pills for sale online nembutal pills for sale online pharmacies are in the industry of improving the health and lives of patients rather than becoming the "henchman" for state governments. https://hospitableending.com/
    "Why should compounders be forced to now play henchman to the ever-hungry executioner," said Foa. "Good compounders want to improve the lives and health of patients; they don't wish to be mired in execution drug controversies, forced to mix drugs to kill prisoners in dangerous and experimental executions."
  • Bonjour,

    Quand vous allez dans "Etat de connexion" l'application vous indique que la communication ne passe pas entre :

    - l'application avec Internet ?
    - Internet avec le contrôleur ?
    - Contrôleur avec équipements ?

    Pouvez vous m'indiquez le code PIN de votre contrôleur puis activer la télémaintenance svp ?

    Dans l'attente de votre réponse.


    Ronan
Recommended